This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD251: Does it meet ISO11898-1 and CAN2.0A?

Part Number: SN65HVD251

Hi Team,

Does the SN65HVD251 meet ISO11898-1 and CAN2.0A?

Thanks!

Roy

  • Roy,

    ISO11898-1 is the CAN and CAN FD frame format for the protocol, which is irrelevant to the transceiver itself. The transceiver is just the physical layer that translates the logic waveform from the controller to a CAN bus waveform on the CANH and CANL pins, and then translates from CAN bus to logic signal to the controller as well. SN65HVD251 can facilitate classical CAN communication.

    The same is true for CAN2.0A as well, this is a protocol definition that is agnostic to the transceiver itself. 

    Please let us know if you have any other questions. Also, what application will this be going into?

    Regards,

    Eric Hackett