This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: RGMII RX timing

Part Number: DP83822I


Hi! 

I'm trying to add timing constraints on the FPGA side, which is receiving RX data from the DP83822I PHY.

I'm going for 100Mbps.

Question 1: 

Figure 7-12 contains both SetupT and SetupR:

Why is both SetupT and SetupR in the figure? 

Is SetupR/HoldR trying to describe the valid window at the FPGA (receiver)? (making assumptions about our PCB?)

Question 2: 

(In chapter 7.16, the following is specified: 

SetupR = min 1 ns,

HoldR = min 1 ns )

Based on SetupR and HoldR, it seems that the data valid window is only 1+1 = 2 ns, even though the clock period is 40 ns (for 100Mbps mode).

Did I interpret this correctly? It seems a bit narrow.

Question 3: 

In the table for SetupR etc: since we constrain for worst-case, I assume that we should ignore the "TYP" column and only use the "MIN" column, right?