Part Number: TCAN4550
Hi,
I have an evaluation board of TCAN4550 FD. My problem is that TCAN4550 seems not answering to the commands.
For test purposes I'm sending 0x41 (read command) 0x00 0x00 (address) 0x01(1 word to be read) following a dummy word 0xFFFFFFFF that should allow TCAN to answer.
Address 0000 should contain the datas 'T' 'C' 'A' 'N'
Attached are the screens of the command issued in the pin n#5 of TCAN4550 (pin n#14 of the eval board's J16 connector ) and the drive of CS (pin #18 of the eval board's J16 connector)
Image 1.jpg contains the CLK vs the MasterOutSlaveInput (pin n#14 of J16)

Image 2.jpg contains CLK vs the CS (pin 18 of j16)

Image3 simp4ly shows that the bit is clocked out at the rising edge of the clock

I performed the same test trying to set dummy byte to 0x000000 instead of 0xFFFFFFFF but nothing happened.
The pin 16 of j16 stays fixed low during all the duration of spi transmit.
I also tried to press the reset button and the wake button but no changes.
VIO select jumper is selecting 3.3 (so compatible with my SPI master)
All the other pins (except for SDI SDO SCLK and CS) are not used in the board and are floating.
Can anybody help me solve the issue?
Thanks