Part Number: SN65DP159
Other Parts Discussed in Thread: TMDS181
Hi Team,
My customer wants to replace TDMS181 with SN65DP159. Does the schematic and Driver code need to be changed?Any things should take into consideration?
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The DP159 is AC coupled input and intend to be used with a AC-coupled HDMI or DP++ source. The TMDS181 is a DC-coupled input and intend to be used with a DC-couple HDMI source.
You can replace the TMDS181 with the DP159, but you have to add AC coupling caps and 50ohm to 3.3V termination on the input. When you add 50ohm termination to 3.3V, the input signal amplitude will be cut in half which the source has to compensate.
Thanks
David