Other Parts Discussed in Thread: DP83TC811EVM, DP83822I, DP83TD510E
To Sreenivasa,
Hello
I have same question about the other PHY board : DP83TD510EVM (2 boards assembly : DP83TD510E plugged on DP838221), same functional board than DP83TC811EVM but speed is less (10Mbps). I suppose the issue is the same : Master and slave configuration, but on this one the default config is : DP83TD510E in RMII Master Mode, DP83822I in RMII Slave Mode (default from the user guide)
Do I need to change these setting on one board to have then the configuration as :
Board 1 : DP83TD510E in RMII Master Mode, DP83822I in RMII Slave Mode
Board 2 : DP83TD510E in RMII Slave Mode, DP83822I in RMII Master Mode
Thank for your reply
Fab