Part Number: DP83TD510E-EVM
Other Parts Discussed in Thread: DP83TD510E, DP83822I, USB-2-MDIO
Hello,
I do use DP83TD510E in RMII Master Mode, DP83822I in RMII Slave Mode (default) with same config both side of the twisted pair and I would like to know if I should modify the config on the 2nd assembly board as follow :
board 1 : DP83TD510E in RMII Master Mode, DP83822I in RMII Slave Mode (default)
board 2 : DP83TD510E in RMII Slave Mode, DP83822I in RMII Master Mode (default)
If I need to do so, is there a way to switch the boards Master/Slave mode using software instead remove manually resistor/strap ?
Is it possible from the µUSB connector ? If yes were can I found the driver MSP430 (do I need it ?) , the one from the user guide link do not match with the board name and the .inf name, windows7 reject the driver.
Thank
Fab