Part Number: DS280BR810
Hello Expert,
Our customer has questions for DS280BR810 as below.
- Datasheet's VOD LIM-min/Max value means the output amplitude which is achieved by datasheet's test condition
Then, Could we change output amplitude from 360mVpp(0x0B[4:0]=0x00, 0x0D[3:0]=0x0,0x0C[3:0]=0x0,0x06[0]=0x1,0x06[7:6]=0x3) to 1260mVpp(0x0B[4:0]=0x1F, 0x0D[3:0]=0x0,0x0C[3:0]=0x0,0x06[0]=0x1,0x06[7:6]=0x3) by only changing 0x0B register manually? - If 1st question's understanding is correct, Does it mean can we configured output amplitude as 31step(29mVpp/step)?
- For 0x06[7:6], could we regard these resister is same principle as 0x0B?
Would you answer for these questions?
I'm looking forward to haring back from you.
Best regards,
Kazuki Kuramochi