Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UB935-Q1,
Hello together,
I'm wondering what is happening if there is an error in the backchannel from the DS90UB954-Q1 if it is used together with the DS90UB935-Q1? So if there is an error in the FPD link between the deserialiser and the serialiserI an CRC error should occur. If this error occurs ist there only the flag set and the errorcounter incremented or ist there any error handling implemented directly? Is the wrong data just transferred further on or will it be deleted just to wait for an new packet?