This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1048AV-Q1: TCAN1048AVDRQ1: ESD data request

Part Number: TCAN1048AV-Q1

Hi Support Team.

I am creating a delivery specification for this part number.

In the Qualification Summary, the results of ESD-HBM and CDM are described as "See data sheet".
However, the datasheet does not show the results of ESD.


Please tell me ESD data (HBM data , CDM data) of TCAN1048AVDRQ1.

Thanks,

  • Yutaro,

    TCAN1048 devices actually share a datasheet with TCAN1046 for all device variants. I have provided a snippet from the TCAN1046 datasheet with HBM and CDM ESD data. 

    HBM class 3A = +-3000V

    HBM class 3B = +-10000V

    CDM = +-750V

    Regards,

    -Tyler