Part Number: PCA9543A
Hi
Customer want to confirm if this device can support this application, see image below.

Thank you in advance.
Regards,
Maynard
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Maynard,
I can't recommend this configuration. This switch is controlled via I2C commands to the SDA/SCL port. It will not recognize commands send from the SD0/SC0 or SD1/SC1 ports unless these channels are enabled. Because all channels are disabled by default, there would not be a way for either host device to communicate with the switch after a power-on reset. A layout should be used that allows a host device to communicate with the SDA/SCL port of the switch in order to control and configure the device after startup.
Let us know if you have any more questions. If not, please let us know by clicking the green resolved button.
Regards,
Eric Schott