Part Number: DP83TD510E
Hi,
1. I would like to work with this PHY in an industrial area which allows only ATEX approved devices. Does this Ethernet-APL chip meet with any explosion safety standards or requirements? If I would like to use this PHY on a custom made board equipped with PoDL, do you have any guidelines how to design it to be explosion safe? Thanks in advance!
2. Do you have a preprogrammed Profinet/Modbus TCP Stack which can be used with this PHY? I would like to use Profinet/Modbus TCP protocol with this chip but without reimplementing the whole protocol from scratch. Or maybe a tested library wich would run on an STM32 or similar MCU?
3. Do you have Ethernet-APL PHY with integrated MAC interface like Analog Devices has: https://www.analog.com/media/en/technical-documentation/data-sheets/adin1110.pdf ?
Thanks in advance!
Regards
Karoly Poka