Part Number: TUSB8044AEVM
Hi,
Is there a way to work with the TUSB8044AEVM without the external 5v?
meaning working with the host USB power?
Thanks,
Itay
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB8044AEVM
Hi,
Is there a way to work with the TUSB8044AEVM without the external 5v?
meaning working with the host USB power?
Thanks,
Itay
Hi Itay,
The TUSB8044AEVM is not designed to be bus powered since max power consumption on a single USB 3.0 port is 900 mA, which doesn't allow enough power for the hub to be powered and to supply power up to 900 mA to each of its downstream ports. An external power supply is required for normal operation.
Regards,
JMMN
Hi JMMN,
Thanks for the reply.
In my application we will draw only 20mA from each port. My question is if in such case we can run the EVB without external power supply.
Thanks again,
Itay
Hi Itay,
While the application you describe is not compliant to the USB specification, if you have a closed system and a USB host port that can power both the EVM and the downstream devices, you can modify the EVM to run from bus power . We did not include onboard switch option to enable a bus power mode.
Regards,
JMMN