This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TG720EVM-MC: Common mode choke for the 1000BASE-T1

Part Number: DP83TG720EVM-MC

Hi,
I think that wrong part for the DP83TG720G on the EVM board.
The common mode choke used is DLW32MH201XK2L, which is actually meant for 100BASE-T1:
For 1000BASE-T1, it is recommended to use DLW32MH101XT2L:
Based on sdd21, the loss at 600MHz is quite substantial:
Please help to advice if this is valid or any reason DLW32MH201XK2L is used.
Regards,
Teoh