This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2036: Will it support SPI is 20MHz and I2C is 1.34MHz

Part Number: TUSB2036
Other Parts Discussed in Thread: TUSB4020BI, TUSB4041I

HI,

if we connected  6MHz crystal to 29 & 30 pins, will it operate at 48 MHz?.

: if this HUB has 48MHz operation, will it support all frequencies less than 48MHz?, because  my SPI is 20MHz and  I2C is 1.34MHz.