Hello
I'm tring to interface the DS90UB954 with a DS90UB933. I already tested the 933 board with a good link with the corrisponding 934 deserializer. For interfacing with a MIPI SoC board, I want to use a 954 deserializer and I developped a board with this device. The link seems to be good so PASS and LOCK are ok. The 933 is driven directly by a 48MHz clock sourced by the sensor.
In the 933 I set the MODE to work in 12-bit mode with Rpu of 15K and Rpd of 56K (1.42V). In 954 the same.
What I'm facing is that on regs 0x73/0x74 I read the correct Line numbers but in 0x75/0x76 I read exactly 1.5 times the line lenght. Is this correct?
Thanks