Part Number: TPS25750
The following relate the the charge current settings in the TPS25750 GUI
- Questionnaire: 3. What is the required sink power or power consumed?
- Advanced Configuration: Sink PDOs
My question then is what is the order of preference of the settings for the PDO? For instance does #1 set the minimum power required for the device to negotiate a sink event? Are the PDOs in #2 requested in order of preference (ie: request the highest number PDO(7,6,5,4, etc) from the list(in #2) that is also advertised as a source capability from the source)?
Nick