Part Number: HD3SS215
May I confirm HD3SS215 's operation temperature for NFBGA package? The information was missing in the datasheet.

or we should simply follow the below section in the datasheet for different packages?

Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: HD3SS215
May I confirm HD3SS215 's operation temperature for NFBGA package? The information was missing in the datasheet.

or we should simply follow the below section in the datasheet for different packages?

Thanks.
Hi,
For commercial temperature range: 0°C to 70°C
For Industrial temperature range: –40°C to 85°C
Thanks
David