Part Number: DS90UB964-Q1
Dear person,
Please advise me on my questions bellows.
I consider using DS90UB964 with four DS90UB935s.
I concern that the one CSI-2 output port can support outputting the video
data transferred from four DS90UB935s.
One XSI-2 port can run at 1.6Gbps/lane. Using four lanes, the bandwidth
is 6.4 Gbps.
However, I there may be some overhead such as LP00-LP11 transition, inter packet gap etc.
Q1. Can you let me know how much percent of bandwidth can be allocated to the payload (video data)?
Q2. If one CSI-2 output port can not handle the maximum input data, can you use two CSI-2 output port
to extend the output bandwidth?
Mita