Part Number: TCA9545A
Hi Sir:
I am very confuse about Vih max in datasheet 6.3 Recommended Operating Conditions describe.
according to table 6.3 appear that Vih is 0.7Vcc~ Vcc+0.5.
Now my question is that my circuitry is connect VCC of TCA9545A Vcc to power rail 2.5V.
function pin A1 and INT3~INT0 pull to VCC 3.3V via resistor.
Here the Vih 3.3V> (2.5V+0.5V) and exceed max requirement.
it was very interesting why Vih is refer to Vcc+0.5 v not 6V.
Are there side any about my design?
Thanks,