Part Number: TCA9535
Hello Expert,
Could you help to check the IO state when we set it as a input? What’s value of impedance in IO pin?

thanks
Jim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9535
Hello Expert,
Could you help to check the IO state when we set it as a input? What’s value of impedance in IO pin?

thanks
Jim
Jim,
When the I/O is set as an input, the pin is put into a High-Z state. There are no internal pullup resistors to pull to VCC or GND. Looking at the input leakage current spec from the datasheet, we can expect the impedance of the I/O to ,change as the input voltage changes. At max conditions, assume Ileak = 1uA and VCC=5.5V, we can calculate that the impedance of the I/O pin is VCC/Ileak >= 5.5Mohm.
Regards,
-Tyler