Hi,
About TPD3S014-Q1,the recommended design is to connect to D+D-, I would like to ask if it can connect to CC1/CC2 and why
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
About TPD3S014-Q1,the recommended design is to connect to D+D-, I would like to ask if it can connect to CC1/CC2 and why
thanks
Hi, Hazel,
1. USB2.0 high speed bit rate is 480Mbps, USB C PD bit rate is 300Kbps. From signal integration, it can be used for CC pins.
2. From operation voltage level perspective, we can see the Vrwm is higher than CC operation voltage level, and no OVP protection on D1 and D2 pin.
From above two point, I think this part can be used for CC1 and CC2 IEC ESD protection.
Bob