Part Number: TPS65988EVM
Hello,
I'm new to PD and I'm trying to make our application work with this EVM.
Requirements:
- One port sinks 20V to power the system
- One port sources 5-20V
- The two ports are interchangeable
Some dynamic allocation, battery charger etc. is probably required later, but I'm trying to make the simple version work first.
I can't get this to work on the EVM. The EVM can negotiate the proper contract from the supply. The EVM can also source 5-20V as negotiated by another USB PD device but only when powered via the barrel connector, not when powered from the other USB port.
Could you please advise how to configure this?