Part Number: TSER953
Other Parts Discussed in Thread: TDES954
I have a TDES954 and a TSER953 setup with a coax connection, and the V3Link connection seems stable -- I'm able to talk to both chipsets, toggle GPIOs, etc. I have the TSER953 connected to an OV2740 sensor with two data lanes and the connections are very short on the board. I'm getting CSI-2 errors -- namely the reading from register 0x5E I'm reading 0x44, which is "Lane 0/1: Multi-bit Error in SYNC Sequence - Uncorrectable". That error sounds pretty bad, but I'm wondering A) what could cause it and B) if this is truly uncorrectable (i.e. there's something fundamentally wrong) or if that just means the chip is unable to correct it, but it may be correctable with a change of passives or something along those lines.
Thanks,
luis