Part Number: HD3SS3212
Hi,
in my design I am using HD3SS3212IRKST multiplexer in followed configuration:
USB Type-C Receptacle (Connection for Host e.g. Notebook/PC) -> Mux HD3SS3212IRKST -> Connector for USB 3.0 Device (e.g. camera)
My Device is not recognized by notebook at all no matter if connect USB-Type C cable in one direction or other (flipped/unflipped).
My question is how do I have to correctly connect SuperSpeed signals for device side and host side using HD3SS3212IRKST Mux?
In my attached schematic link you can see how I connected everything please note that SEL is floating but during testing I connected it to GND or 3V3 but still no recognition of USB 3.0 Device.
What I tested and figured out so far:
- It doesn't matter if I use termination caps (220nF) on Tx1_P/Tx1_N & Tx2_P/Tx2_N or not populated them and route through = Device is not recognized by Host
- if I swap connections on device side like that A0P = TXP, A0N=TXN, A1P=RXP, A1N=RXN (just manually with wires most likely not impedance conform) = I get at least a windows message from Host that Device is not recognized properly (Connection Status ->Device failed enumeration)
What I can rule out as errors:
- USB 3.0 Device Camera (testes with other hardware)
- PCB Impedance (report is available)
SCHEMATIC
Thanks a lot!