Part Number: TPS25750
Other Parts Discussed in Thread: USB-PD-CHG-EVM-01, , BQ25792
Hello,
I've been working with the USB-PD-CHG-EVM-01 to show it working as a proof of concept for our battery. One thing that will be important for our application is to have the ability to separately disable sinking and/or sourcing (more sinking, but in error conditions we'll want to stop sourcing as well).
I was hoping that the GPIO on the TPS25750 could be used for this, but slvuc05.pdf only outlines a few input functions (none of which seem applicable). Is it possible to do this over I2C? Or something else that I'm missing?
Thanks,
-Eric