This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Device recommendation



Hello team,

can you suggest the best device we can offer for my customer's HDMI application below? 

HDMI Solution.zip

1. The application is for Karaoke mixer amplifier, 4 HDMI in, 2 HDMI output
2. Need 4 port HDMI input for the machine, one is selected source each time
3. Selected input source, audio will send to DSP with I2S format
4. The output from DSP will back to the target chip with I2S format
5. Audio from DSP will combine with select Video the output as HDMI
6. Request HDMI 4.0

Regards,

Renan