Part Number: TPS65988EVM
Hi,
In our design PD controller is connected with MCU via I2C lines. MCU has to do some control activity depending on the PD controller status. PD controller will be connected with 2 USB devices that are capable of sending the command to the MCU via VDM. How does the MCU identify which device has sent the VDM(Device 1 or Device 2)? Both the USB devices will have the common firmware and can send the command anytime depending on their own state.