Other Parts Discussed in Thread: DAC8760, DAC8740H, DAC8830
Dear Sir/Madam,
I am getting some issue while using DAC8760IPWPR for 4-20mA generator and DAC8740HRGET for HART communication
if initialize as 4-20mA option in DAC 8760 without Enabling HART in config register it is working fine ,
but when I am initializing HART (Enabling by setting config register 0x57 to 0x0010) it will lift my 4-20mA signal by 6.6mA
for example 4mA -> 10.6mA and 5mA -> 11.6 and so on upto 20mA -> 26.6mA and in this situation my HART communication
Working fine.