This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

duplicate 24bit RGB



Hi team,

One of our customers has the following needs:

A group of CMOS 3.3V BUS (24bit RGB parallel port video, RGB[23:0], P_CLK, HS, VS, P_CLK, speed 150MHz) are copied into two groups and output to two receivers, mainly considering the signal driving ability and the reflection of the isolating receiver. The two output channels need to be valid at the same time. Does TI have such a solution?

Best Regards,

Amy Luo