Part Number: SN65LBC031
Other Parts Discussed in Thread: SN75LBC031, SN65HVD251
Hello team,
I have three questions for SN65LBC031.
1. The datasheet describes that "The SN75LBC031 is a CAN transceiver used as an interface between a CAN controller and the physical bus for high speed applications of up to 500 kBaud".
But on the TI.com page, SN65LBC031 supports up to 1MHz. Which is correct value?
2. My customer is considering to use SN65LBC031QDR instead of SN65HVD251DR.
Rs pin (Mode select) of SN65HVD251DR is set by 1kΩ pulldown. To achieve similar spec with SN65LBC031QDR, how to set ASC pin?
3. Do you think this replace is no problem? P2P device is must be needed so I proposed The SN75LBC031.
Best regards,
Shotaro