Part Number: TCA9535
Other Parts Discussed in Thread: TCA9555
Hello
we are using the TCA9535 and we have about 8 of the 16 pins as unused in our design. The unused pins to not have the Pullup or Pull down through 10k (GND or VCC). In our design we see the USED pins being driven ON at Power Up. Indicating that the device is powering up with its pins partially driven (seems to be weak drive) to a HIGH state. This behavior is of course not what the datasheet indicates (all pins are configured as INPUTs at power up). Can you tell us if we add the resistor pullup/down (10k) to these unused pins that the partially driven ON state on the USED pins will be alliiviated?
I have attached our connectivity of the part in our application below
TCA9535 configuration We are using TCA9535RTWR Pin 20 : SDA : 10K Pullup to +3.3V : Driven By FPGA (sink drive) after power up Pin 19 : SDL : 10K Pullup to +3.3V : Driven By FPGA (sink drive) after power up Pin 22 : INT : 10K Pullup to +3.3V : No other connection Pin 21 : VCC : Direct connecto +3.3V : FPGA uses same supply Pin 24,23,18: A2:A0 : Connected to GND Pin 9,EPAD: GND:EPAD: Connected to GND Pin 1: P00 : Connected to LVTTL xcvr input pin (+3.3V). No other connection Pin 2: P01 : Connected to LVTTL xcvr input pin (+3.3V). No other connection Pin 3: P02 : Connected to 10K series R to 2N2222 BJT Base. A 100k base resistor to GND is also used. No other connections Pin 4: P03 : Connected to parallel a 10k to GND. P03 drives a LVC logic input (+3.3V). No other connections Pin 5: P04 : P04 drives a LVC logic input (+3.3V). No other connections Pin 6,7,8: P05:P07 : No connections Pin 10: P10 : Drives Gate of 2N7002 N-Ch MOS Pin 11: P11 : Drives Gate of 2N7002 N-Ch MOS Pin 12: P12 : Drives Gate of 2N7002 N-Ch MOS Pin 13-17 P13:P17 : No connections
Can you assist
Thanks, Tom