Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550
Hi,Ti Friend
I have some questions about TCAN4550-Q1.
1.What is the meaning of the abbreviation'INT',e.g. TXD_INT,RXD_INT,are they all means 'interrupt' or what?
2.In normal mode, nINT pin will pull low when any of interrupt coming?GPO1 pin can be map to M_CAN_INT 1(it means when M_CAN_INT 1 come, GPO 1 will active low
), GPO 2 pin can be map to M_CAN_INT 0(it means when M_CAN_INT 0 come, GPO 2 will active low),is that right?
3.How to understand M_CAN_INT 0 and M_CAN_INT 1,what does they really mean?
4.How to understand interrupt line in TCAN4550,what are the relationships between interrupt line and GPO1,GPO2,or nINT pin?
Looking forward to an answer.
Best regards.
Jianhua