Part Number: TPS65987DJEVM
Other Parts Discussed in Thread: TIDA-050014, TPS65987DDJ
Hi team,
I have a question about Configuration setting of TPS65987DJEVM. and I connect to the TIDA-050014 which is sink.
I have two different setting, please see below figure.


The difference is the Source PDO 4 maximum current. One is 3A, the other is 2.5A.
When the PDO 4 maximum current is 3A. I put the 20V bottom, the voltage will increase to 20V/3A.
When the PDO 4 maximum current is 2.5A. I put the 20V bottom, the voltage will increase to 15V/3A, not what I set.
Could team give me some advice? I don't no why. Do I set wrong register?