This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83825I: Throughput performance

Part Number: DP83825I

Hello,

 

My customer has some question for DP83825I.

 

1.

I think it highly depends on the host processor performance, what protocol is used and network environment, but they want to know how much throughput could be achievable with DP83825i in 100Mbps mode.

Do we have any benchmark result?

 

2.

DP83825 has some modes for clock input, 25MHz and 50MHz, Master and Slave.

Is there any difference between each mode for actual throughput?

 

3.

DP83825 has only RMII I/F, but for example DP83822 have MII, RMII and RGMII.

Is throughput performance different between them?

 

Regards,

Oba