This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: DP83869HM Fiber Output Signal Levels

Part Number: DP83869HM

Hi Team,

I'm using DP83869HM in media converter mode. While taking waveforms of SOP,SON signals , I realize that my waveform parameters are not matching with those given in datasheet.

Concern parameters are

- Rise and fall time (I'm getting them as 16ns and 1.4ns resp)

-clock frequency (i'm getting 63MHz)

-Peak-peak voltage (I'm getting 1.27 v)

As per datasheet these should be ---- 

Also , what is the significance of ( Configuration bits for 0.6V -1.8V ) . Any other parameters should i check. ?

Please guide.