Part Number: TUSB8043A
Hi,
In App Note SLLA414(August 2018), the recommendation is like this, namely that the length and spacing of the sawtooth should be larger than 3W and 2A, respectively.

However, other sources are recommending differently:
NXP recommends the spacing to be LESS:

Altium and Toradex recommends both the width and spacing should be less:


Which is correct?