This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you share the scope plot? Are you connecting the output to 50ohm termination to 3.3V?
Thanks
David
Dipali
Looking at the schematic, why do you have LCD_B5 connected to DATA0/1/7 and LCD_G5 connected to DATA8/9/15, and LCD_R5 connected to DATA16/17/23?
Can you double check the HPD and make sure the HPD is driven high?
Thanks
David
Thanks for the Reply. We are using 18 bit LCD, but now I have modified my mistake I connect LSB of each color to Ground. Still same Issue. I think HPD is detected monitor, because when I coonnect it to Monitor blue light glows it shows No signal, but after some time it disappeared.
Regards
Dipali
Dipali
Can you probe the clock output? Are you seeing a valid clock frequency?
Are you setting BSEL high and use single-edge clocking?
Thanks
David
CLK output from RGB signal is proper. BSEL connected to 3.3V throught 4.7K resistor.
Regards
Dipali
Dipali
Can you also measure the TXC+/- clock frequency? What is the resolution you are trying to support? Are you seeing a valid clock output on TXC+/-?
Thanks
David
No output at TXC+/- clock Frequency. .Resolution I am trying is 1920 x 1080 pixel.
Regards
Dipali
Dipali
When you measured the TXC+/- clock frequency, do you have the output connected to 50ohm termination to 3.3V? The TXC+/- output needs to see 50ohm termination to 3.3V in order to have a valid output.
Thanks
David
Hi,
Can you please provide the scope plot of the TXC+/- and HPD?
Do you have 5V on the mini-HDMI connector?
Thanks
David