Other Parts Discussed in Thread: TUSB8020B
Hi everyone,
First of all thank you for your time. I am new in the USB world so forgive me if I get some terminology wrong.
We are designing a board that has a controller with one USB3.0 port (upstream) that should receive data from two USB2.0 High Speed devices simultaneously at 300Mbps each:

For example, the TUSB8020B would achieve that topology. But if I have understood the datasheet correctly the TUSB8020B does not translate the USB2.0 lines to the Superspeed differential pairs. So receiving 300Mbps from each device at the same time would saturate the 2.0 lines, right? Ideally I would like an IC (or circuit) that would translate the 2.0 lines into the Superspeed lines. Would this be possible?
Something similar to this (although it is only a 1:1 translator I think it shows what I want): www.via-labs.com/product_show.php
I am having some troubles finding a suitable chip/solution for my problem from bigger suppliers.
I hope I managed to explain my problem clearly.
Best regards and thank you for your time,
Iñigo