Part Number: TFP401A
Other Parts Discussed in Thread: TFP401
Hello.
I am using the TFP401A to receive an hdmi stream ...
I made all the development tests using TFP401PZP Evaluation Module ...and I found no difficulties ...
I realized the board (as in the picture) ...
but unfortunately the TFP401A doesn't output any signal (Vsync Hsync DE) ... except the ODCK
I give you some data:
the card has the ground plane ...
when the hdmi cable is connected I notice an increase in current consumption of about 200 mA due to the activities of TFP401
I enclose a picture of the board in the connection part of the connector - TFP401
wiring diagram...
I ask you some questions
is it possible that my Layout of RX0 RX1 RX2 RXC pairs is wrong ?...
the differential pairs RX0 RX1 RX2 RXC must have all the same length?
can you help me to solve the problem?
best regards
Giovanni Pitino