Part Number: MAX3232-EP
Other Parts Discussed in Thread: STRIKE, MAX3232
Hi, TI Support Team
A request for schematic review has been received from a customer.
I request a review of the circuit diagram below.

Thanks.
Regards,
MJ
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi MJ,
The capacitors are correctly wired and are of correct value to adjust the charge pump circuitry.
ROUT2 does not need a 4.7kohm pullup resistor since driving architecture on that pin is push-pull configuration.
The 33ohm series resistance may be a good call in terms of fault protection such as a short-circuit fault or in protecting against an ESD strike, but since ROUT2 abs max is -0.3V to VCC + 0.3V you may consider taking out the series resistance. Also keep in mind that the series resistance on ROUT2 creates a low-pass filter with parasitic capacitance to ground, attenuating your data signal to the MCU. I don't know the length of cable between the MAX3232 to MCU, but this could mess with signal integrity.
Other than these suggestions, I think the over schematic looks good.
Regards,
-Tyler