Part Number: TPD4E1U06
Other Parts Discussed in Thread: ESD224
Hi Team,
I have some questions about ESR protection device,
My customer using Amazing's ESD protection AZC099-04SC.R7G. and I do the comparable table.
but it seems like TI's product cannot compete to Amazing (IEC 61000-4-5).
Does Team has any suggestion on ESD protection device?
Because my customer want to have p2p solution, all I can find is TPD4E1U06 which is the best device in TI.com.
| AZC099-04SC.R7G | TPD4E1U06 | |
| Vendor | Amazing | Texas Instruments Inc |
| Capacitance | 1pF | 0.8pF |
| IEC 61000-4-2 (ESD) | ±15-kV Contact Discharge,±15-kV Air-Gap Discharge | ±15-kV Contact Discharge,±15-kV Air-Gap Discharge |
| IEC 61000-4-2 | 40 A (5/50 ns) | 80 A (5/50 ns) |
| IEC 61000-4-5 | 5.5 A (8/20 μs) | 3 A (8/20 μs) |
| Channel | quad-channe | quad-channeㄠ |
| Package | SOT-23-6L | SOT-23 |
This figure is block diagram of monitor.