Part Number: TCA9800
Other Parts Discussed in Thread: TCA9617A
Hi,
As subject.
I check datasheet, they're P2P, only operation voltage range different.
I would like to know could TCA9617A drop in replace TCA9800 without any BOM change?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jim,
TCA9800 and TCA9617A are p2p compatible. TCA9617A VCC is 0.8V to 5.5V. TCA9800 VCC is 0.8V to 3.6V.
TCA9800 only needs pull-up resistors to VCC on the A-side only. B-side does not need pull-up resistors.
TCA9617A will need pull-up resistors on both A and B sides.
Regards,
Tyler