Part Number: SN65C1167
Other Parts Discussed in Thread: UCC21710,
Dear E2E Team
I am using SN65C1167EPWR in UCC21710 based Gate Driver Board as suggested in the following link.
https://www.wolfspeed.com/cgd1700hb2m-una
The input is a differential input for SN65C1167 IC.
My query is Can I replace the IC with TC4426/4427 IC? Switching frequency in my application is 100kHz.
Doing so, I won't be using the driver in differential configuration. Are there any drawbacks of not using in differential mode? What are the advantages of using differential driver?
Distance between my Controller board and Gate Driver board is 15".
Best Regards