Other Parts Discussed in Thread: DS90UR241
I am currently analyzing a fault condition with the following behavior:
First the deserializer works as expected. The transmitted camera image is shown correctly. Deserializers LOCK and PASS outputs are HIGH.
An event/condition, which we do not yet know, causes that we just get a white screen instead of the camera image.
In this condition we still measure 3.3V (#1) at the outputs LOCK and PASS. Even if we then physically disconnect the FPD-Link Signal, we still measure 3.3V (#1) at LOCK and PASS.
#1: due to pull-ups in our application, LOCK and PASS remains HIGH or go to TRI-STATE.
So is there a typical reason that causes this kind of behavior?
application details:
Camera data is serialized via DS90UR241. A DS90UR910 in backward compatible mode deserializes the stream.