Part Number: SN65DP159
Hi all!
I want to use the SN65DP159 48 pin for an HDMI output from my FPGA.
The problem is, that my FPGA only has two outputs left, so I want to use a 2 lane display port,
to send to the SN65DP159 and get a 4 lanes LVDS signal out for my HDMI.
My question is, is this possible, and if this is possible must I use the AUX to select how many channels I want to use?
Also if this is possible must I attach the two DP lanes to pins In_D0p, In_D0n & In_D1p, In_D1n?
Many thanks.
Kind regards,