Part Number: TUSB9261
I understand that there is no TUSB9261 Programmers Guide that is available to non TI developers, but would it be possible to provide information on just one register? I am trying to slow the SPI clock speed and from the source code I can see that it is set by a field in the SPI_FMT0 register. I would greatly appreciate it if you could provide information on the size, location, and definition of the bit fields in that register.
Thanks
Eric