Part Number: TUSB1002A
Hi TI,
We're using the TUSB1002A (TUSB1002AIRGET) in a design and would like to verify our implementation of the redriver chip is correct.
The goal of the design is to allow Superspeed or superspeedplus signals (5Gb/s or 10Gb/s) to pass from the Host (via USB3 Type-B Receptacle) through the TUSB1002A redriver and then onto a USB3 Type-C Receptacle.
We are using two TUSB1002A because we would like to pass superspeed or superspeedplus signals to both channels/sides of the USB Type-C receptacle.
Mainly, I'd like to verify that the TUSB1002A will work with Type-B and Type-C receptacles (most application notes/examples have Type-A on both sides of the redriver).
Also, do the Superspeed signals look like they are oriented correctly?
In the TUSB1002A schematic checklist, it states the following:

In our implementation, we are connecting the redriver to USB receptacles so we may have the superspeed signals reversed (i.e. SSTX of the host connected to SSRX input of the redriver).
Do you see any issues with our implementation of the TUSB1002A?
Sincerely,
Cameron Bolton