Part Number: TCA9539-Q1
Other Parts Discussed in Thread: TCA9539,
Dear Expert,
I want to know when the TCA9539's I2C is disrupted, the GPIO will remain output level or reset to the power-on state?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9539-Q1
Other Parts Discussed in Thread: TCA9539,
Dear Expert,
I want to know when the TCA9539's I2C is disrupted, the GPIO will remain output level or reset to the power-on state?
Thanks!
Haibin,
In the event of a time-out or improper operation, the system controller can reset the TCA9549-Q1 by asserting an active low input to the RESET input. This will put registers back to their default state setting I/O's to inputs and initializing the I2C-SMBus state machine.
Regards,
Tyler
The output pins will change only at the ACK bit (that is, at the 27th or 36th clock edge) at the end of the register write (see figure 8-9).
A STOP condition will end the transaction. If the STOP condition is corrupted, the following clock cycles might be seen by the TCA9539-Q1 as the last part of the write transaction.