Part Number: DP83822I
Hello,
In DP83822I PHY Two types of LED_0 driving connections are possible,
1. LED_0 Pin in Sink mode - Pull-Up Configuration

2. LED_0 Pin in Source mode - Pull-Down Configuration
Which configuration is recommended as per TI?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83822I
Hello,
In DP83822I PHY Two types of LED_0 driving connections are possible,
1. LED_0 Pin in Sink mode - Pull-Up Configuration

2. LED_0 Pin in Source mode - Pull-Down Configuration
Which configuration is recommended as per TI?
Hi Rohidas,
Both configurations are valid. It just depends on what the user would like to bootstrap the pin into. These pins during power-up and resetting turn into inputs where they sample the voltage. The voltage measured at that point in time tells the PHY what mode to go into upon bring-up. The LED_0 pin controls the AN_0 bit, whose information is located in Table 8-11. Depending on the mode you would like the PHY in, please strap LED_0 (AN_0), RX_D0 (AN_D1), RX_D3 (AN_EN), and COL (FX_EN) accordingly.
Sincerely,
Gerome