This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC812S-Q1: How to connect VSLEEP, INH, CLKOUT if not used?

Part Number: DP83TC812S-Q1

Hello Team,

How to connect VSLEEP, INH, CLKOUT  in DP83TC812S-Q1 if these pins are not used?

Piotr 

  • Hi Piotr,

    The pins need to be connected in the following ways:

    - VSleep: 3.3V with 0.1uF capacitors. This is a power supply connection so this must be connected.

    - INH: This is an output that is used when implementing TC-10. It will be high for all states except TC-10 Sleep mode. If TC-10 is being used, a pull-down resistor must be used.

    - CLKOUT: This is a pin which outputs a 25MHz clock waveform. It is commonly used for debugging purposes, so atleast bringing it out to a test point is advised for system development and debugging. 

    Sincerely,

    Gerome